Configuring: Delete Fields
Select which fields within the dataset need to be deleted. Note that it is not possible to delete all fields of the dataset, and that when a field is deleted, the entire column is deleted, not only the values.
Steps to configure
-
Field selection: Select which fields must be deleted.
-
Execute: The selected fields will be removed from the dataset.
Step 1: Field selection
Select the fields you would like to delete.
-
Not all fields can be selected for deletion.
-
Default: All fields are listed in the available window.
-
Minimum configuration: At least one field needs to be selected.
Step 2: Execute
The selected field columns will be completely removed from the dataset.
Related topics: